NET_PRES_TransSignalHandlerDeregister Type
C
typedef bool (* NET_PRES_TransSignalHandlerDeregister)(NET_PRES_SKT_HANDLE_T handle, NET_PRES_SIGNAL_HANDLE hSig);
Returns
true - Indicates success
false - Indicates failure
Description
Transport Layer Deregister Handler Function Pointer Prototype This function is called by the presentation layer when the application wants to deregister a handler function.
Preconditions
A socket needs to have been opened by NET_PRES_TransOpen.
Parameters
Parameters | Description |
---|---|
handle | The handle returned from NET_PRES_TransOpen. |
hSig | The handler handle returned from NET_PRES_TransHandlerRegister. |