NET_PRES_SocketSignalHandlerDeregister Function
C
bool NET_PRES_SocketSignalHandlerDeregister(NET_PRES_SKT_HANDLE_T handle, NET_PRES_SIGNAL_HANDLE hSig);
Returns
true - If the call succeeds
false - If no such handler is registered
Description
This function calls the transport layer's deregister signal handler function, if it exists
Preconditions
A socket needs to have been opened by NET_PRES_SocketOpen.
Parameters
Parameters | Description |
---|---|
handle | The presentation layer socket handle. |
hSig | A handle returned by a previous call to TCPIP_TCP_SignalHandlerRegister. |