4.13.4 Spanning Tree CIST Ports Configuration
The STP CIST Port Configuration page allows you to inspect the current STP CIST port configurations and set physical and aggregated ports.
The STP CIST Port Configuration page has the following parameters:
- CIST Aggregated/Normal Port Configuration
- Port: The switch port number of the logical STP port
- STP Enabled: Controls whether STP is enabled on this switch port
- Path Cost: Controls the path cost incurred by the port. The Auto setting sets the path cost as appropriate by the physical link speed, using the 802.1D recommended values. Using the Specific setting, a user-defined value can be entered. The path cost is used when establishing the active topology of the network. Lower path cost ports are chosen as forwarding ports in favor of higher path cost ports. Valid values are in the range of 1–200000000.
- Priority: Controls the port priority. This can be used to control priority of ports having identical port cost. Lower priority is better.
- Admin Edge: Controls if the operEdge flag must start as set or cleared (the initial operEdge state when a port is initialized).
- Auto Edge: Controls if the bridge must enable automatic edge detection on the bridge port. This allows operEdge to be derived from whether BPDUs are received on the port or not.
- Restricted Role: If enabled, this causes the port not to be selected as Root port for the CIST or any MSTI, even if it has the best spanning tree priority vector. Such a port is selected as an Alternate port after the Root port has been selected. If set, it can cause lack of spanning tree connectivity. It can be set by a network administrator to prevent bridges external to a core region of the network from influencing the spanning tree active topology, possibly because those bridges are not under the full control of the administrator. This feature is also known as Root Guard.
- Restricted TCN: If enabled, it causes the port not to propagate received topology change notifications and topology changes to other ports. If set, it can cause temporary loss of connectivity after changes in a spanning tree's active topology because of persistently incorrect learned station location information. It is set by a network administrator to prevent bridges external to a core region of the network, causing address flushing in that region, possibly because those bridges are not under the full control of the administrator or the physical link state of the attached LANs transits frequently.
- BPDU Guard: If enabled, it causes the port to disable itself upon receiving valid BPDUs. Contrary to the similar bridge setting, the port Edge status does not affect this setting. A port entering error-disabled state due to this setting is also subjected to the bridge Port Error Recovery setting.
- Point-to-Point: Controls whether the port connects to a point-to-point LAN rather than to a shared medium. This can be automatically determined or forced either true or false. Transition to the forwarding state is faster for point-to-point LANs than for shared media.