1.1.2.1.1.3.35 BLE_GAP_ExtAdvParams_T
C
typedef struct BLE_GAP_ExtAdvParams_T
{
uint8_t advHandle;
uint16_t evtProperies;
uint32_t priIntervalMin;
uint32_t priIntervalMax;
uint8_t priChannelMap;
BLE_GAP_Addr_T peerAddr;
uint8_t filterPolicy;
int8_t txPower;
uint8_t priPhy;
uint8_t secMaxSkip;
uint8_t secPhy;
uint8_t sid;
bool scanReqNotifiEnable;
} BLE_GAP_ExtAdvParams_T;Description
Extended advertising parameters.
Field Documentation
| Field | Description |
|---|---|
| advHandle | Identifies the advertising set whose parameters are being configured (Range: 0 to 0xEF). See Maximum advertising handle. |
| evtProperies | The type of advertising event that is being configured and its basic properties. The bit combination of Event type of advertising report. |
| priIntervalMin | Minimum advertising interval, (Range: 0x20 to 0x1F4000). (Unit: 0.625 ms) See Extended primary advertising interval. |
| priIntervalMax | Maximum advertising interval, (Range: 0x20 to 0x1F4000). (Unit: 0.625 ms) See Extended primary advertising interval. |
| priChannelMap | Advertising Channel Map. See Advertising channel BLE_GAP_ADV_CHANNEL_ALL can't be used. |
| peerAddr | Remote bluetooth address and address type, see BLE_GAP_Addr_T. |
| filterPolicy | Advertising filter policy. See Advertising filter policy. |
| txPower | The maximum power level at which the advertising packets are to be transmitted on the advertising channels. Set to 0x7F if user has no perference of extended advertising TX power level. Level will be adjusted if value is not in range. |
| priPhy | Indicates the PHY on which the advertising packets are transmitted on the primary advertising channel. 2M can't be used for primary advertising. See PHY type. |
| secMaxSkip | The maximum number of advertising events that can be skipped before the AUX_ADV_IND can be sent. |
| secPhy | Indicates the PHY on which the advertising packets are transmitted on the secondary advertising channel. See PHY type. |
| sid | The value to be transmitted in the Advertising SID subfield of the ADI field of the Extended Header. See Advertising SID range. |
| scanReqNotifiEnable | Indicates whether the notifications shall be sent upon the receipt of a scan request PDU. Set true to enable notification. Set false to disable notification. |