15.5.2.2.4 LLC Resonant Converter Mode
Support for LLC resonant converter topologies is provided within the PWM hardware. This mode should be operated in push-pull output mode. Therefore, there are two PWM timer cycles, one active PWMxH and the other for PWMxL. To maintain stability, the intent of this mode is to capture the on time of the first half and apply it to the second half while maintaining dead time.
-
The capture event can occur before or after the existing period count such that PGxCAP ≤ PGxPER. Captures that occur in this range may cause both outputs to remain low in the cycles following this capture.
- If no PCI event occurs, then EOC will be considered as a capture event.
- Software capture is not applicable in LLC mode.
Control is done on a cycle-by-cycle basis using a PCI input to truncate the high time of
the PWMxH and the period of the first half of the cycle (when PGxSTAT.STEER =
0). When the PCI event occurs, the hardware captures the period
value (period1) for use on the second half.
Period1 = PGxCAP +1
The contents of PGxPER are unaffected as PGxPER is used as an upper period limit in the case of no PCI truncation event. If no PCI event occurs, Period1 = PGxPER +1.
The hardware also calculates the effective high time of PWMxH. It is defined as:
HighTime = Period1 - DTH
The period and resulting high time of the second half (PGxSTAT.STEER =
1) is then calculated:
Period2 = HighTime + DTL
The 2nd half of the cycle data then becomes Period2, DTL and HighTime.
Restrictions:
- This Operating mode is not available in HR because the period boundary must coincide with the PWM clock cycle.
- A PCI event within the DTH will result is both outputs being low.
-
The PCI override as selected in CAPSRC[2:0] is disabled. The system can rely on the other PCI events for override.
- PGxDCA is not applicable in LLC mode.
- LLC mode must be used with the Push-Pull Output mode.