2.4 Buck Converter Guidelines and Considerations

A buck converter is implemented on the dsPIC33AK256MPS306 device family. The buck allows for reduced power loss and heat generated within the device. The connections are:

  • SWVDD – This power pin is connected to the internal power switches of the buck converter. This pin has high transient currents and should have a low impedance path to VDD. A 10 µF (4.7 µF minimum) capacitor is recommended as close as possible to the pin.
  • SWVSS – This power pin is connected to the internal power switches of the buck converter. This pin has high transient currents and should have a low impedance path to the PCB ground.
  • LX - This pin is the output of the H bridge power switches and provides current to the external inductor. This pin has high transient currents and should have a low impedance trace to the inductor.
  • VDDCORE – This pin supplies power from the external inductor to the core. A 10 µF capacitor is required and should be placed as close to the VDDCORE pin and inductor as possible.

The buck converter adjusts the duty cycle to maintain a constant voltage output as the current demands change. Current is delivered to the core through the external inductor and is filtered with the capacitor in the VDDCORE pin. Figure 2-1 illustrates a simplified topology of the buck components inside the dsPIC®.

Figure 2-1. Buck Regulator Topology

No other connections should be made to the VDDCORE or LX pins. The output voltage of the buck converter is listed in Electrical Characteristics. An example application circuit is shown in Figure 2-2.

Figure 2-2. Example Application Circuit