6.2.3.6 Import Atmel Project - Summary
Step 6 or 7. Summary
Review the summary before clicking Finish. If anything is incorrect, use the Back button to go back and change it.
When the project is being imported, observe any warnings or other messages in the Output window. You may need to make changes so your new project will build.
The new project will open in the Projects window.
Note: The source files from the original
Atmel project are linked, as opposed to copied. So modifications to the source files in
either the Atmel or MPLAB X IDE projects will be noticed in
both.