Exception During Unsuccessful BOOTSWP Operation
If timing of an exception during BOOTSWP execution meets that outlined in Figure 7-4, and the BOOTSWP criteria are not met, the panel swap will not occur. Exception processing will, therefore, vector into the current active panel, and the handler will return to the address following the BOOTSWP in that panel as normal.