Panel Swap Code Sequence
For a successful BTSEQ validation, a prior instruction (to BOOTSWP) is responsible for reading and loading the inactive panel BTSEQ number into a W-reg. The BOOTSWP instruction must operate on the same register to validate the value read.
The boot sequence number is a 12-bit unsigned value. The BTSEQ word format consists of two 12-bit values with BTSEQ [11:0] containing the true sequence number, and BTSEQ [23:12] containing its complement as shown in Figure 7-4. BTSEQ [127:24] is reserved and must read as all 0’s.
Panel Swap Code Example shows a panel swap example code.
Panel Swap Code Example
// Boot sequence number addresses
// BTSEQ is the first word of the last row
#define BTSEQ_ACTIVE_ADDR (__PROGRAM_BASE + __PROGRAM_LENGTH - 0x10UL)
#define BTSEQ_INACTIVE_ADDR (0x400000UL | BTSEQ_ACTIVE_ADDR)
// Inactive partition reset vector address
#define INACTIVE_RESET_VECTOR_ADDR (0x400000UL | __RESET_BASE)
// BTSEQ - Partition 1 boot sequence number
#define BTSEQ_1 0x10
uint32_t __attribute__((space(prog), address(BTSEQ_ACTIVE_ADDR))) btseq_1 = (~(uint16_t)BTSEQ_1 << 12) | (BTSEQ_1);
// BTSEQ - Partition 2 boot sequence number
#define BTSEQ_2 0x20
uint32_t __attribute__((space(prog), address(BTSEQ_INACTIVE_ADDR))) btseq_2 = (~(uint16_t)BTSEQ_2 << 12) | (BTSEQ_2);
void __attribute__((address(__PROGRAM_BASE), keep, noinline)) partition_swap(void)
{
asm volatile("\n mov.sl #%0, w1"
"\n mov.l [w1], w1" // w1 = Inactive Partition FBTSEQ value (first word of last row)
"\n mov.sl #%1, w0"
"\n mov.l [w0], w0" // w0 = Inactive Partition reset vector destination (__reset label on Inactive Partition)
"\n bootswp w1"
// must use CALL instruction since partition_swap() creates a new stack frame
// if the function does not create a new stack frame using the LNK instruction,
// a GOTO instruction should be used instead of the CALL instruction
"\n call w0"
: /* no outputs */ : "i"(BTSEQ_INACTIVE_ADDR), "i"(INACTIVE_RESET_VECTOR_ADDR) : "w0", "w1");
}
If the BOOTSWP is enabled and the BTSEQ validation succeeds, BOOTSWP will be successful, and it will result in a panel swap and SR.Z = 1 and NVMCON.SOFTSWAP = 1.
If BOOTSWP is enabled but the BTSEQ validation fails, BOOTSWP will be unsuccessful. To indicate this result to subsequent code, BOOTSWP will drive SR.Z = 0. NVMCON.SOFTWAP will also not be set.
If BOOTSWP is not enabled but execution is attempted, no error will be flagged, and the instruction will execute as if a two-cycle NOP. Execution will then continue as normal (from the same panel).
The BOOTSWP instruction will always be fetched from the original active panel mapping. The instruction immediately following BOOTSWP may be any instruction other than another BOOTSWP and will be fetched from either the new or current active panel, depending upon the success or failure of the BOOTSWP operation.
Successful BOOTSWP: The CPU will attempt to fetch the instruction following BOOTSWP but will be stalled by the PBU. The PBU will then invalidate the cache and ISB. When complete, the original instruction fetch will be allowed to proceed but from the new active panel.
Unsuccessful BOOTSWP: The instruction following BOOTSWP will be fetched and executed as normal from the current active panel.
Should the user need to switch back and forth between panels at any point, code located at label (see Panel Swap Code Example) should test SR.Z or the NVMCON.SOFTSWAP status bit to determine whether or not the BOOTSWP was successful, then take the appropriate action. For applications where a one way swap is required, code at label”= in the current active panel can assume an unsuccessful panel swap and take appropriate action. Code at the same address within the new active panel can jump directly to the application code, knowing that the panel swap must have succeeded.
- Successful execution of the BOOTSWP instruction will not reload the configuration registers, so those of the original active panel will be persistent.
- It is the responsibility of the user software to accommodate an unsuccessful operation.
- Other than providing a mechanism to swap the panel order within address space, we do not facilitate the panel swap in any other way within the device. The user is wholly responsible to guarantee application data coherency, timing, recovery, etc.
Figure 7-5 shows a BOOTSWP instruction flow diagram.
Figure 7-6 shows a panel swap sequence flow diagram