25.4.1.6 Asynchronous Transmitter Mode
The module is, by default, configured as an asynchronous transmitter. In this mode, the module continuously transmits message frames as long as the ON bit is set (SENTxCON1[15]). The final falling edge of the CRC nibble also serves as the first falling edge of the Sync pulse. An interrupt is generated at the completion of the CRC nibble.
Figure 25-4 and Figure 25-5 show the relationship between the control, status and interrupt events.
- Tick Time, TTICK (Equation 25-1)
- Number of data nibbles, N
- Hardware or application calculated CRC
- Use of pause period for a fixed message period
- The overall duration of the SENT Message if the pause period is present (Equation 25-2).
- Clear RCVEN (SENTxCON1[11]) for Transmit mode.
- Clear TXM (SENTxCON1[10]) for asynchronous transmit.
- Write the value of the desired frame length to NIBCNT[2:0] (SENTxCON1<2:0>).
- Set or clear CRCEN (SENTxCON1[8]) to configure the module for hardware or software CRC calculation.
- Write the value for the desired TICKTIME to SENTxCON2.
- If the optional pause period is required, set PPP (SENTxCON1[7]) to enable the feature, then write the value of FRAMETIME to SENTxCON3.
- Enable the SENT interrupt(s) and set the interrupt priority.
- Write the initial status and data values to SENTxDATA. If application-based CRC
is being used (CRCEN =
0), also calculate the message CRC and write it to CRC<[:0]. - Set ON (SENTxCON1[15]) to enable the module.
Updates to SENTxDATA must be performed after the completion of the CRC and before the next message frame’s status nibble. The recommended method is to use the message frame completion interrupt to trigger data writes.
SENT1 Asynchronous Transmission Code
#include <stdio.h>
#include <stdlib.h>
#include <xc.h>
#define mFclk (4E+6)
#define mTickTime (70E-6)
#define mFrameTime (25E-3)
int main(void) {
_RP26R = 81; // Assign SENT1OUT to pin RP26
SENT1CON1bits.RCVEN = 0; // Module operates as a transmitter
SENT1CON1bits.TXM = 0; // Asynchronous Transmit
SENT1CON1bits.NIBCNT = 6; // 6 data nibbles per data packet
SENT1CON1bits.CRCEN = 1; // CRC is calculated using the J2716 method
SENT1CON1bits.PPP = 1; // SENTx messages transmitted with Pause Pulse
SENT1CON1bits.PS = 0; // Module clock is FSENT
SENT1CON2 = ( (mTickTime * mFclk) - 1); // TICKTIME
SENT1CON3 = ( mFrameTime / mTickTime) ; // FRAMETIME
_SENT1IE = 1; // Enable SENT1 interrupt
_SENT1IP = 4; // SENT interrupt priority
SENT1DATbits.STAT = 0; // Status Nibble
SENT1DATbits.DATA1 = 1; // Data Nibble 1
SENT1DATbits.DATA2 = 2; // Data Nibble 2
SENT1DATbits.DATA3 = 3; // Data Nibble 3
SENT1DATbits.DATA4 = 4; // Data Nibble 4
SENT1DATbits.DATA5 = 5; // Data Nibble 5
SENT1DATbits.DATA6 = 6; // Data Nibble 6
SENT1CON1bits.ON = 1; // Enable SENT module
while(1);
return 0;
}
void __attribute__((__interrupt__,__auto_psv__)) _SENT1Interrupt (void)
{
_SENT1IF = 0; // Clear interrupt flag
// Update SENT1DAT here
}