16.5.2.6.10 PCI Source Synchronized to EOC, Latched Modes
When the PCI acceptance logic is operated in the Latched mode and
PSYNC = 1, the PCI source is synchronized to the
EOC event, as shown in Figure 16-27. The
synchronization logic delays the rising edge of the PCI source signal until the next
occurrence of the EOC signal. The output of the synchronization logic is deasserted on
the falling edge of the PCI source signal. The output of the synchronization logic is
then used to set the SR latch. A PCI input pulse that operates entirely within one EOC
period will not assert the PCI active signal. This is because the falling edge of the
PCI input signal resets the EOC synchronization logic before an event can be
produced.