17.4.2 Analog Inputs
Any analog input (external pin or internal analog signal) can be mapped to any channel by the PINSEL[3:0] bits (ADnCHxCON1[27:24]) for a positive input and by the NINSEL[1:0] bits (ADnCHxCON1[29:28]) for a negative input. The input can be configured as single-ended or differential using the DIFF bit (ADnCHxCON1[31]) (where n is the specific ADC module and x is the respective channel of the ADC).
The ANSELx registers for the I/O ports associated with the analog input are used to configure the
corresponding pins as analog pins. A pin is configured as an analog input when the
corresponding ANSELx bit = 1. When the ANSELx bit = 0,
the pin is set to digital control. The ANSELx bits are set when the device comes out of
Reset, causing the ADC input pins to be configured as analog inputs by default. The
TRISx registers control the digital function of the port pins. The port pin that is
required as an analog input must have its corresponding bit set in the specific TRISx
register, configuring the pin as an input. If the I/O pin associated with an ADC input
is configured as an output by clearing the TRISx bit, the port’s digital output level
will be converted. After a device Reset, all TRISx bits are set. The PORT register bit
reads as ‘0’ if its corresponding pin is configured as an analog input.
For more information on port pin configuration, refer to “I/O
Ports”.