27.4.5.9 Dead-Time Delay Generator
This section describes the dead-time delay generator that is available on the MCCP module. It is used in specific output modes of the module. The purpose of the dead-time delay generator is to:
- Create two output signals, true and complement, from the single output signal of a PWM generator.
- Provide a brief delay between the time when one signal is driven inactive and the other signal is driven active.
The dead-time delay generator contains edge detectors to monitor input signal transitions and a digital countdown timer. Each time an input signal edge occurs, the countdown timer is loaded with a programmable countdown value specified by the CCPx-CON3.DT[5:0] control bits. The rising edge of the inactive signal is delayed until the countdown timer counts to zero. If DT[5:0] = 0, the dead-time delay generator is effectively disabled and complementary output signals are produced with zero delay between the transitions on each output. A timing diagram for the dead-time delay generator are provided in Figure 27-34.
There are special cases for dead-time generation:
- When the input signal pulse-width is equal to or less than the programmed dead-time value, the desired output results will not be obtained. Figure 27-35 depicts two scenarios where the duty cycle of the input signal is close to 0% and close to 100%. When the duty cycle is close to 0%, both outputs are driven inactive during the dead-time delay period. The out_high signal does not get driven active for any period of time. When the duty cycle is near 100%, both outputs are driven inactive for the dead-time period and the out_low signal does not get driven high for any period of time. These are regions of operation that should be avoided by the user.
- When the input duty cycle is set to 0%, there will be no transitions on the input signal. The out_high signal should remain LOW, and the out_low signal should remain HIGH.
- When the input duty cycle is set to 100%, there should be no transitions on the input signal. The out_high signal should remain HIGH, and the out_low signal should remain LOW.
As the input duty cycle approaches 0% or 100%, the dead-band delay time becomes a more significant portion of the input signal pulse-width. This effect causes a non-linear behavior between the requested duty cycle and the actual system response. Systems that are sensitive to this non linearity must avoid regions near 0% and 100% duty cycle, or use output feedback to compensate the duty cycle.