3 Implementation
(Ask a Question)The PCIe core uses several embedded blocks that are built using Libero configurators. PCIESS functionality is reserved for the Quad0 transceiver block, and this functionality allows up to two x1 or x2 PCIe endpoint/root ports links or one x4 PCIe endpoint/root port link. PCIe 0 and PCIe 1 blocks can be used in any combination of x1 and x2 links within Quad0. A PCIe x4 link is only supported using PCIe 1, PCIe 0 is unused. The Libero configurator allows the setting of the reference clock and data rates for the PCIe block. This information is used to generate the configuration settings for the PMA as well as associated interface logic. The configurators build the components that are used to instantiate/configure specific hardware macros including the PMA and PCS blocks using the Libero SmartDesign software.
Lane[0:1] and Lane[2:3] share on-chip hardware resources that create inter-dependency between the physical lanes. The possible combinations for implementing and mixing the PCIe controllers on four physical XCVR lanes within QUAD0 are shown in the following figure.