3.21 LEDs
The SAM9X75 cHybrid features one RGB LED and eight user LEDs. The LED cathodes are controlled via GPIO pins.
The following figure shows the RGB and user LEDs.
The following table shows the RGB and user LEDs signal descriptions.
| PIO | Signal Name | Signal Description |
|---|---|---|
| PC14 | RGB_LED_RED | Red LED |
| PC21 | RGB_LED_GREEN | Green LED |
| PA22 | USER_LED_1 | Green LED |
| PB0 | USER_LED_2 | Green LED |
| PA7 | USER_LED_3 | Green LED |
| PC15 | USER_LED_4 | Green LED |
| PC28 | USER_LED_5 | Green LED |
| PC27 | USER_LED_6 | Green LED |
| PC29 | USER_LED_7 | Green LED |
| PB17 | USER_LED_8 | Green LED |
| PC20 | RGB_LED_BLUE | Blue LED |