4.7.2.3 To Edit a Breakpoint Location
- In the Breakpoints
window, right click a breakpoint, then click Location on the right click
menu.
—or—
In a source, Disassembly, or Call Stack window, right click a line that contains a breakpoint glyph. Then click Location from Breakpoints on the right click menu.
Note:You must right click the correct character where the breakpoint is set in a source window. Do this if the breakpoint is set on a specific character within a line of source code.