1.1.8.4.17 DRV_SPI_TRANSFER_EVENT Enum
C
typedef enum
{
/* Transfer request is pending */
DRV_SPI_TRANSFER_EVENT_PENDING ,
/* All data were transfered successfully. */
DRV_SPI_TRANSFER_EVENT_COMPLETE ,
/* Transfer Handle given is expired. It means transfer
is completed but with or without error is not known.
In case of Non-DMA transfer, since there is no possibility
of error, it can be assumed same as DRV_SPI_TRANSFER_EVENT_COMPLETE */
DRV_SPI_TRANSFER_EVENT_HANDLE_EXPIRED ,
/* There was an error while processing transfer request. */
DRV_SPI_TRANSFER_EVENT_ERROR ,
/* Transfer Handle given is invalid */
DRV_SPI_TRANSFER_EVENT_HANDLE_INVALID
} DRV_SPI_TRANSFER_EVENT;
Summary
Identifies the possible events that can result from a transfer add request.
Description
This enumeration identifies the possible events that can result from a transfer add request caused by the client calling either DRV_SPI_ReadTransferAdd or DRV_SPI_WriteTransferAdd or DRV_SPI_WriteReadTransferAdd functions.
Remarks
Either DRV_SPI_TRANSFER_EVENT_COMPLETE or DRV_SPI_TRANSFER_EVENT_ERROR is passed in the "event" parameter of the event handling callback function that the client registered with the driver by calling the DRV_SPI_TransferEventHandlerSet function when a transfer request is completed.
When status polling is used, any one of these events is returned by DRV_SPI_TransferStatusGet function.