1.1.8.4.18 DRV_SPI_TRANSFER_EVENT_HANDLER Typedef
C
typedef void (*DRV_SPI_TRANSFER_EVENT_HANDLER )( DRV_SPI_TRANSFER_EVENT event, DRV_SPI_TRANSFER_HANDLE transferHandle, uintptr_t context );
Summary
Pointer to a SPI Driver Transfer Event handler function
Description
This data type defines the required function signature for the SPI driver transfer event handling callback function. A client must register a pointer using the transfer event handling function whose function signature (parameter and return value types) match the types specified by this function pointer in order to receive transfer related event calls back from the driver.
The parameters and return values are described here and a partial example implementation is provided.
Parameters
| Param | Description |
|---|---|
| event | Identifies the type of event |
| transferHandle | Handle identifying the transfer to which the event relates |
| context | Value identifying the context of the application that registered the event handling function. |
Returns
None.
Example
void APP_MyTransferEventHandler( DRV_SPI_TRANSFER_EVENT event,
DRV_SPI_TRANSFER_HANDLE transferHandle,
uintptr_t context )
{
MY_APP_DATA_STRUCT pAppData = (MY_APP_DATA_STRUCT) context;
switch(event)
{
case DRV_SPI_TRANSFER_EVENT_COMPLETE:
{
// Handle the completed transfer.
break;
}
case DRV_SPI_TRANSFER_EVENT_ERROR:
default:
{
// Handle error.
break;
}
}
}Remarks
If the event is DRV_SPI_TRANSFER_EVENT_COMPLETE, it means that the data was transferred successfully.
If the event is DRV_SPI_TRANSFER_EVENT_ERROR, it means that the data was not transferred successfully.
The transferHandle parameter contains the transfer handle of the transfer request that is associated with the event.
The context parameter contains the a handle to the client context, provided at the time the event handling function was registered using the DRV_SPI_TransferEventHandlerSet function. This context handle value is passed back to the client as the "context" parameter. It can be any value necessary to identify the client context or instance (such as a pointer to the client's data) of the client that made the transfer add request.
The event handler function executes in interrupt context of the peripheral. Hence it is recommended of the application to not perform process intensive or blocking operations with in this function.
The DRV_SPI_ReadTransferAdd, DRV_SPI_WriteTransferAdd and DRV_SPI_WriteReadTransferAdd functions can be called in the event handler to add a transfer request to the driver queue. These functions can only be called to add transfers to the driver instance whose event handler is running. For example, SPI2 driver transfer requests cannot be added in SPI1 driver event handler. Similarly, SPIx transfer requests should not be added in event handler of any other peripheral.