1.1.8.4.5 DRV_SPI_TransferSetup Function
C
bool DRV_SPI_TransferSetup ( DRV_HANDLE handle, DRV_SPI_TRANSFER_SETUP * setup )
Summary
Sets the dynamic configuration of the driver including chip select pin. Application must call this API and configure the transfer parameters before starting any data transfers.
Description
This function is used to update any of the DRV_SPI_TRANSFER_SETUP parameters for the selected client of the driver dynamically. For single client scenario, if GPIO has to be used for chip select, then calling this API with appropriate GPIO pin information becomes mandatory. For multi client scenario where different clients need different setup like baud rate, clock settings, chip select etc, then also calling this API is mandatory.
Note that all the elements of setup structure must be filled appropriately before using this API.
Preconditions
DRV_SPI_Open must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| *setup | A structure containing the new configuration settings |
Returns
None.
Example
// mySPIHandle is the handle returned by the DRV_SPI_Open function. DRV_SPI_TRANSFER_SETUP setup; setup.baudRateInHz = 10000000; setup.clockPhase = DRV_SPI_CLOCK_PHASE_TRAILING_EDGE; setup.clockPolarity = DRV_SPI_CLOCK_POLARITY_IDLE_LOW; setup.dataBits = DRV_SPI_DATA_BITS_16; setup.chipSelect = SYS_PORT_PIN_PC5; setup.csPolarity = DRV_SPI_CS_POLARITY_ACTIVE_LOW; DRV_SPI_TransferSetup ( mySPIHandle, &setup );
Remarks
None.