1.2.11.4.22 SYS_TIME_TimerStop Function

1.2.11.4.22 C

SYS_TIME_RESULT SYS_TIME_TimerStop ( SYS_TIME_HANDLE handle )

1.2.11.4.22 Summary

Stops a running software timer.

1.2.11.4.22 Description

This function stops a previously created and running software timer (i.e., the given timer's counter will stop incrementing).

1.2.11.4.22 Precondition

The SYS_TIME_Initialize must have been called and a valid handle to the software timer to be stopped must be available.

1.2.11.4.22 Parameters

ParametersDescription
handleHandle to a software timer instance

1.2.11.4.22 Returns

SYS_TIME_SUCCESS if the operation succeeds.

SYS_TIME_ERROR if the operation fails (due, for example, to an invalid handle).

1.2.11.4.22 Example

Given a "timer" handle, the following example will stops the timer's counter running.

SYS_TIME_TimerStop(timer);

1.2.11.4.22 Remarks

Calling SYS_TIME_TimerStop on a timer that is not running will have no affect and will return SYS_TIME_SUCCESS.