1.2.11.4.29 SYS_TIME_CALLBACK Typedef

1.2.11.4.29 C

typedef void (*SYS_TIME_CALLBACK ) ( uintptr_t context );

1.2.11.4.29 Summary

Pointer to a time system service callback function.

1.2.11.4.29 Description

This data type defines a pointer to a time service callback function. Therefore, defining the function signature. Callback functions may be registered by clients of the time service either when creating a software timer or using the SYS_TIME_Callback shortcut functions.

1.2.11.4.29 Precondition

The time service must have been initialized using the SYS_TIME_Initialize function before attempting to register a SYS Time callback function.

1.2.11.4.29 Parameters

ParametersDescription
contextA context value, returned untouched to the client when the callback occurs. It can be used to identify the instance of the client who registered the callback.

1.2.11.4.29 Returns

None.

1.2.11.4.29 Example

//"MY_APP_DATA_STRUCT" is a user defined data structure with "isTimerExpired" as
//one of the structure members.
void MyCallback ( uintptr_t context )
{
    MY_APP_DATA_STRUCT* pAppData = (MY_APP_DATA_STRUCT *) context;

    if (pAppData != NULL)
    {
        pAppData->isTimerExpired = true;
    }
}

1.2.11.4.29 Remarks

None.