1.2.11.4.10 SYS_TIME_CounterGet Function
1.2.11.4.10 C
uint32_t SYS_TIME_CounterGet ( void )
1.2.11.4.10 Summary
Get the common 32-bit system counter value.
1.2.11.4.10 Description
Returns the current "live" value of the common 32-bit system counter.
1.2.11.4.10 Precondition
The SYS_TIME_Initialize function should have been called before calling this function.
1.2.11.4.10 Parameters
None.
1.2.11.4.10 Returns
The current "live" value of the common 32-bit system counter.
1.2.11.4.10 Example
uint32_t timeStamp1; uint32_t timeStamp2; uint32_t timeDiffMs; // Take first time stamp timeStamp1 = SYS_TIME_CounterGet(); //Perform some tasks.... // Take second time stamp timeStamp2 = SYS_TIME_CounterGet(); //Calculate the time difference. Use the appropriate function - //SYS_TIME_CountToMS or SYS_TIME_CountToUS to calculate the time difference. timeDiffMs = SYS_TIME_CountToMS((timeStamp2 - timeStamp1));
1.2.11.4.10 Remarks
The value returned may be stale as soon as it is provided, as the timer is live and running at full frequency resolution (as configured and as reported by the SYS_TIME_FrequencyGet function). If additional accuracy is required, use a hardware timer instance.