1.2.11.4.21 SYS_TIME_TimerStart Function
1.2.11.4.21 C
SYS_TIME_RESULT SYS_TIME_TimerStart ( SYS_TIME_HANDLE handle )
1.2.11.4.21 Summary
Starts a software timer running.
1.2.11.4.21 Description
This function starts a previously created software timer.
1.2.11.4.21 Precondition
The SYS_TIME_Initialize must have been called and a valid handle to the software timer to be started must be available.
1.2.11.4.21 Parameters
| Parameters | Description |
|---|---|
| handle | Handle to a software timer instance |
1.2.11.4.21 Returns
SYS_TIME_SUCCESS if the operation succeeds.
SYS_TIME_ERROR if the operation fails (due, for example, to an invalid handle).
1.2.11.4.21 Example
Given a "timer" handle, the following example will start the timer's counter running.
SYS_TIME_TimerStart(timer);
1.2.11.4.21 Remarks
Calling SYS_TIME_TimerStart on an already running timer will have no affect and will return SYS_TIME_SUCCESS.
Calling SYS_TIME_TimerStart on a timer that is stopped, will always restart the timer from it is initial configured timer/counter value and will not resume the timer from the counter value at which it was stopped.