1.2.11.4.20 SYS_TIME_TimerCounterGet Function

1.2.11.4.20 C

SYS_TIME_RESULT SYS_TIME_TimerCounterGet (
    SYS_TIME_HANDLE handle,
    uint32_t *count
);

1.2.11.4.20 Summary

Gets the elapsed counter value of a software timer.

1.2.11.4.20 Description

This function gets the elapsed counter value of the software timer identified by the handle given.

1.2.11.4.20 Precondition

The SYS_TIME_Initialize must have been called and a valid handle to the software timer must be available.

1.2.11.4.20 Parameters

ParametersDescription
handleHandle to a software timer instance
countAddress of the variable to receive the value of the given software timer's elapsed counter. This parameter is ignored when the return value is not SYS_TIME_SUCCES.

1.2.11.4.20 Returns

SYS_TIME_SUCCESS if the operation succeeds.

SYS_TIME_ERROR if the operation fails (due, for example, to an invalid handle).

1.2.11.4.20 Example

Given a "timer" handle, the following example will get the given software timer's elapsed counter value.

uint32_t count;

if (SYS_TIME_TimerCounterGet(timer, &count) != SYS_TIME_SUCCESS)
{
    // Handle error
}

1.2.11.4.20 Remarks

The counter value may be stale immediately upon function return, depending upon timer frequency and system performance.