DRV_W25_GeometryGet Function
C
bool DRV_W25_GeometryGet( const DRV_HANDLE handle, W25_GEOMETRY *geometry );
Summary
Returns the geometry of the device.
Description
This API gives the following geometrical details of the W25 Flash:
- Number of Read/Write/Erase Blocks and their size in each region of the device
- Flash block start address
Precondition
The DRV_W25_Open() routine must have been called for the specified W25 driver instance.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| *geometry_table | Pointer to Flash device geometry table instance |
Returns
True - If able to get the geometry details of the Flash.
False - If read device id fails.
Example
DRV_HANDLE handle; // Returned from DRV_W25_Open DRV_W25_GEOMETRY w25FlashGeometry; uint32_t readBlockSize, writeBlockSize, eraseBlockSize; uint32_t nReadBlocks, nReadRegions, totalFlashSize; DRV_W25_GeometryGet(handle, &w25FlashGeometry); readBlockSize = w25FlashGeometry.read_blockSize; nReadBlocks = w25FlashGeometry.read_numBlocks; nReadRegions = w25FlashGeometry.numReadRegions; writeBlockSize = w25FlashGeometry.write_blockSize; eraseBlockSize = w25FlashGeometry.erase_blockSize; totalFlashSize = readBlockSize * nReadBlocks * nReadRegions;
Remarks
This API is more useful when used to interface with Memory driver.