DRV_W25_ReadJedecId Function
C
bool DRV_W25_ReadJedecId( const DRV_HANDLE handle, void *jedec_id );
Summary
Reads JEDEC-ID of the Flash device.
Description
This function schedules a blocking operation for reading the JEDEC-ID. This information can be used to get the Flash device geometry.
Precondition
The DRV_W25_Open() routine must have been called for the specified W25 driver instance.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
Returns
True - If the read is successfully completed.
False - If read jedec-id command fails.
Example
DRV_HANDLE handle; // Returned from DRV_W25_Open
uint32_t jedec_id = 0;
if(DRV_W25_ReadJedecId(handle, &jedec_id) == false)
{
// Error handling here
}
Remarks
This routine will block wait for transfer to complete.