DRV_W25_PageWrite Function

C

bool DRV_W25_PageWrite( const DRV_HANDLE handle, void *tx_data, uint32_t tx_data_length, uint32_t address );

Summary

Writes one page of data starting at the specified address.

Description

This function schedules a non-blocking write operation for writing maximum one page of data into Flash memory.

The requesting client should call DRV_W25_TransferStatusGet() API to know the current status of the request.

Preconditions

The DRV_W25_Open() routine must have been called for the specified W25 driver instance. The Flash address location which has to be written, must have been erased before using the W25_xxxErase() routine. The Flash address has to be a Page aligned address.

Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open routine
*tx_dataThe source buffer containing data to be programmed into W25 Flash
tx_data_lengthTotal number of bytes to be written. should not be greater than page size
addressWrite memory start address from where the data should be written

Returns

True:

  • if the write request is successfully sent to the Flash

False:

  • if Write enable fails before sending sector erase command to Flash
  • if write command itself fails

Example

#define PAGE_SIZE    256
#define BUFFER_SIZE  1024
#define MEM_ADDRESS  0x0

DRV_HANDLE handle;  // Returned from DRV_W25_Open
uint8_t CACHE_ALIGN writeBuffer[BUFFER_SIZE];
bool status = false;

if(false == DRV_W25_SectorErase(handle))
{
    // Error handling here
}

// Wait for erase to be completed
while(DRV_W25_TransferStatusGet(handle) == DRV_W25_TRANSFER_BUSY);

for (uint32_t j = 0; j < BUFFER_SIZE; j += PAGE_SIZE)
{
    if (DRV_W25_PageWrite(handle, (void *)&writeBuffer[j], (MEM_ADDRESS + j)) == false)
    {
        status = false;
        break;
    }

    // Wait for write to be completed
    while(DRV_W25_TransferStatusGet(handle) == DRV_W25_TRANSFER_BUSY);
    status = true;
}

if(status == false)
{
    // Error handling here
}

Remarks

This routine will block wait until write request is submitted successfully.

Client should wait until write is complete to send next transfer request.