4.1 Installation of the GUI
(Ask a Question)To install the GUI, perform the following steps:
- Extract the contents of the
mpf_an4664_df.zipfile. From thempf_an4664_df\GUIfolder, double-click thesetup.exefile. - Follow the instructions displayed on the installation wizard.
After successful installation, PCIe_Root_Port_GUI appears on the Start menu of the host PC desktop. If the GUI application is not yet installed, see Prerequisites section.