25.8.5 Interrupt Enable Set
Name: | INTENSET |
Offset: | 0x0E |
Reset: | 0x0000 |
Property: | PAC Write-Protection |
Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | |
SEEWRC | SEESOVF | SEESFULL | |||||||
Access | R/W | R/W | R/W | ||||||
Reset | 0 | 0 | 0 |
Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
SUSP | NVME | ECCDE | ECCSE | LOCKE | PROGE | ADDRE | DONE | ||
Access | R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W | |
Reset | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit 10 – SEEWRC SEE Write Completed Interrupt Enable
Writing a zero to this bit has no effect.
Writing a one to this bit sets the SEEWRC interrupt enable.
This bit will read as the current value of the SEEWRC interrupt enable.
Bit 9 – SEESOVF Active SEES Overflow Interrupt Enable
Writing a zero to this bit has no effect.
Writing a one to this bit sets the SEESOVF interrupt enable.
This bit will read as the current value of the SEESOVF interrupt enable.
Bit 8 – SEESFULL Active SEES Full Interrupt Enable
Writing a zero to this bit has no effect.
Writing a one to this bit sets the SEESFULL interrupt enable.
This bit will read as the current value of the SEESFULL interrupt enable.
Bit 7 – SUSP Suspended Write Or Erase Interrupt Enable
Writing a zero to this bit has no effect.
Writing a one to this bit sets the SUSP interrupt enable.
This bit will read as the current value of the SUSP interrupt enable.
Bit 6 – NVME NVM Error Interrupt Enable
Writing a zero to this bit has no effect.
Writing a one to this bit sets the NVME interrupt enable.
This bit will read as the current value of the NVME interrupt enable.
Bit 5 – ECCDE ECC Dual Error Interrupt Enable
Writing a zero to this bit has no effect.
Writing a one to this bit sets the ECCDE interrupt enable.
This bit will read as the current value of the ECCDE interrupt enable.
Bit 4 – ECCSE ECC Single Error Interrupt Enable
Writing a zero to this bit has no effect.
Writing a one to this bit sets the ECCSE interrupt enable.
This bit will read as the current value of the ECCSE interrupt enable.
Bit 3 – LOCKE Lock Error Interrupt Enable
Writing a zero to this bit has no effect.
Writing a one to this bit sets the LOCKE interrupt enable.
This bit will read as the current value of the LOCKE interrupt enable.
Bit 2 – PROGE Programming Error Interrupt Enable
Writing a zero to this bit has no effect.
Writing a one to this bit sets the PROGE interrupt enable.
This bit will read as the current value of the PROGE interrupt enable.
Bit 1 – ADDRE Address Error Interrupt Enable
Writing a zero to this bit has no effect.
Writing a one to this bit sets the ADDRE interrupt enable.
This bit will read as the current value of the ADDRE interrupt enable.
Bit 0 – DONE Command Done Interrupt Enable
Writing a zero to this bit has no effect.
Writing a one to this bit sets the DONE interrupt enable.
This bit will read as the current value of the DONE interrupt enable.