25.8.2 Control B

Name: CTRLB
Offset: 0x04
Reset: 0x0000
Property: PAC Write-Protection

Bit 15141312111098 
 CMDEX[7:0] 
Access PAC Write-ProtectionPAC Write-ProtectionPAC Write-ProtectionPAC Write-ProtectionPAC Write-ProtectionPAC Write-ProtectionPAC Write-ProtectionPAC Write-Protection 
Reset 00000000 
Bit 76543210 
  CMD[6:0] 
Access WWWWWWW 
Reset 0000000 

Bits 15:8 – CMDEX[7:0] Command Execution

This bit group should be written with the key value 0xA5 to enable the command written to CMD to be executed. If the bit group is written with a different key value, the write is not performed and INTFLAG.PROGE is set. PROGE is also set if the a previously written command is not complete.

The key value must be written at the same time as CMD. If a command is issued through the APB bus on the same cycle as an AHB bus access, the AHB bus access will be given priority. The command will then be executed when the NVM block and the AHB bus are idle.

STATUS.READY must be one when the command is issued.

INTFLAG.DONE is set when the command completes.

ValueNameDescription
0xA5 KEY Execution Key
Other - Reserved

Bits 6:0 – CMD[6:0] Command

These bits define the command to be executed when the CMDEX key is written.
ValueNameDescription
0x0 EP Erase Page - Only supported in the User page in the auxiliary space.
0x1 EB Erase Block - Erases the block addressed by the ADDR register, not supported in the user page
0x2 Reserved
0x3 WP Write Page - Writes the contents of the page buffer to the page addressed by the ADDR register, not supported in the user page
0x4 WQW Write Quad Word - Writes a 128-bit word at the location addressed by the ADDR register.
0x5-0xF Reserved
0x10 SWRST Software Reset - Power-Cycle the NVM memory and replay the device automatic calibration procedure and resets the module configuration registers
0x11 LR Lock Region - Locks the region containing the address location in the ADDR register until next reset.
0x12 UR Unlock Region - Unlocks the region containing the address location in the ADDR register until next reset.
0x13 SPRM Sets the power reduction mode.
0x14 CPRM Clears the power reduction mode.
0x15 PBC Page Buffer Clear - Clears the page buffer.
0x16 SSB Set Security Bit
0x17 BKSWRST Bank swap and system reset, if SmartEEPROM is used also reallocate its data into the opposite BANK
0x18 CELCK Chip Erase Lock - DSU CTRL.CE command is not available. As soon as the CELCK command is successfully executed, the chip erase capability is disabled and Microchip’s failure analysis capabilities are limited. Therefore, the software has to ensure there is a way to unlock the chip erase by executing the CEULCK command.
0x19 CEULCK Chip Erase Unlock - The DSU CTRL.CE command is available.
0x1A SBPDIS Sets STATUS.BPDIS, bootloader protection is discarded until CBPDIS is issued or next start-up sequence.
0x1B CBPDIS Clears STATUS.BPDIS, bootloader protection is not discarded.
0x1C-0x2F Reserved
0x30 ASEES0 Configure SmartEEPROM to use Sector 0
0x31 ASEES1 Configure SmartEEPROM to use Sector 1
0x32 SEERALOC Starts SmartEEPROM sector reallocation algorithm
0x33 SEEFLUSH Flush SmartEEPROM data when in buffered mode
0x34 LSEE Lock access to SmartEEPROM data from any means
0x35 USEE Unlock access to SmartEEPROM data
0x36 LSEER Lock access to the SmartEEPROM Register Address Space (above 64KB)
0x37 USEER Unock access to the SmartEEPROM Register Address Space (above 64KB)
0x38-0x7F Reserved