3.3.1.1 Oscilloscope Control Panel
The Oscilloscope control panel is where the oscilloscope is configured and connected to the rest of the system. The control panel has five sections, which are described in detail in the following sections.

The Oscilloscope control panel is where the oscilloscope is configured and connected to the rest of the system. The control panel has five sections, which are described in detail in the following sections.

The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.