3.3.1.1.3 Trigger Controls
The Oscilloscope trigger sub-module helps to identify and lock on to only the portion of the input signal desired. Depending on the operating mode set by the run controls, the trigger can:
-
Lock on to a periodic signal and constantly update the plot
-
Only update the plot when the signal exceeds some level
Edge Triggering
The edge triggering mechanism is looking for the signal to cross the trigger level. For a positive edge trigger, the signal must go from below the trigger level, to above the trigger level.
- No trigger – the line must cross.
- No trigger – wrong direction.
- Trigger point.
- No trigger – the line must cross.
- No trigger – wrong direction.
- Trigger point.
Set the Edge Trigger Type
The trigger mechanism has two edge trigger modes: Positive and Negative Edge Trigger.
- To set the Positive Edge Trigger mode,
click the
button. The button will be highlighted when activated. - To set the Negative Edge Trigger mode,
click the
button. The button will be
highlighted when activated.
Set the Trigger Level
The trigger level can be adjusted in three different ways:
-
Enter a trigger level value into the text box. Press the TAB keyboard button or click the mouse outside the text box to let the new value take effect.
-
Click on the up/down arrows located to the right of the text box
-
With the mouse cursor positioned over the text box, scroll the mouse wheel to increase/decrease the trigger level setting
-
Drag the trigger level line in the plot area to a new position
Select the Trigger Source
The Oscilloscope trigger sub-module uses one of the channel signals when looking for the trigger condition.
-
Click the colored Trigger source button corresponding to the channel chosen for use as a trigger source. The active Trigger source button will be highlighted.
Set the Trigger Mode
- Click Normal to enable Triggered mode. The plot will only be updated when the trigger condition is satisfied.
- Click Auto to enable Free Running mode. The plot will be updated continuously and the trigger conditions will be ignored.