1.17 RTC Periodic Interrupt

This example application shows how to use the RTC to generate periodic interrupts.

Description

This example application demonstrates how to use the 32-bit timer mode of the RTC to generate periodic ticks. It toggles an LED every time the callback is triggered.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file.

Path of the application within the repository is apps/rtc/rtc_periodic_timeout.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32cm_pl10_curiosity_nano.XMPLAB X project for PIC32CM PL10 Curiosity Nano Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameBoard
pic32cm_pl10_curiosity_nano.XPIC32CM PL10 Curiosity Nano Evaluation Kit

Setting Up PIC32CM PL10 Curiosity Nano Evaluation Kit

  • Connect the Debug USB port on the board to the computer using a USB Type-C cable

Running the Application

  1. Build and program the application using its IDE.
  2. The LED blinks continuously.

Refer to the following table for details of LED:

BoardLED Name
PIC32CM PL10 Curiosity Nano Evaluation KitLED0