1.12 PM Wakeup Using EIC
This application demonstrates entering the Low Power modes and exiting it using the EIC.
Description
The PM peripheral library is used to enter the Low Power mode and the device exits Low Power mode when the button is pressed. To identify a button push, the EIC is configured to detect a falling edge on the GPIO pin connected to the switch.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file.
Path of the application within the repository is apps/pm/pm_wakeup_eic.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32cm_pl10_curiosity_nano.X | MPLAB X project for PIC32CM PL10 Curiosity Nano Evaluation Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Board |
|---|---|
| pic32cm_pl10_curiosity_nano.X | PIC32CM PL10 Curiosity Nano Evaluation Kit |
Setting Up PIC32CM PL10 Curiosity Nano Evaluation Kit
- Connect the Debug USB port on the board to the computer using a USB Type-C cable
Running the Application
- Open the terminal application (e.g., Tera term) on the computer.
- Connect to the Curiosity Virtual
COM port and configure the serial settings as follows:
- Baud: 115200
- Data: 8 bits
- Parity: None
- Stop: 1 bit
- Flow Control: None
- Build and program the application using its IDE.
- LED is blinked continuously using the SysTick.
- The console displays the
following message:

- Select
aorbto enter the Low Power mode (the LED is turned OFF when the device enters Low Power mode). - Press the switch to exit the Low Power mode.
- LED will start blinking and the
console displays the following message:

Refer to the following table for details of Switch and LED:
| Board | Switch Name | LED Name |
|---|---|---|
| PIC32CM PL10 Curiosity Nano Evaluation Kit | SW0 | LED0 |