1.8 DMAC USART Echo

This example application demonstrates USART transfer with DMA to receive 10 bytes and echo back the received bytes.

Description

This application demonstrates USART transfer with DMA using SERCOM peripheral configured in USART mode. One DMA channel is used to receive 10 bytes of data from the USART and another DMA channel is used to echo back the received bytes.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file.

Path of the application within the repository is apps/dmac/dmac_usart_echo.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32cm_pl10_curiosity_nano.XMPLAB X project for PIC32CM PL10 Curiosity Nano Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameBoard
pic32cm_pl10_curiosity_nano.XPIC32CM PL10 Curiosity Nano Evaluation Kit

Setting Up PIC32CM PL10 Curiosity Nano Evaluation Kit

  • Connect the Debug USB port on the board to the computer using a USB Type-C cable

Running the Application

  1. Open the terminal application (e.g., Tera term) on the computer.
  2. Connect to the Curiosity Virtual COM port and configure the serial settings as follows:
    • Baud: 115200
    • Data: 8 bits
    • Parity: None
    • Stop: 1 bit
    • Flow Control: None
  3. Build and program the application using its IDE.
  4. The console displays the following message:
  5. Type 10 characters in the console.
  6. Entered 10 characters will be echoed back and the LED is toggled.

Refer to the following table for details of LED:

BoardLED Name
PIC32CM PL10 Curiosity Nano Evaluation KitLED0