1.27 WDT Timeout

This example shows how to generate a Watchdog Timer (WDT) reset by emulating a deadlock.

Description

This example application shows how the WDT peripheral library resets the WDT by not feeding the watchdog on switch press. The application sets up the watchdog to reset the device. The application as well sets up the timer to blink an LED to emulate a process. A user switch press forces the device to wait in an infinite loop to emulate a deadlock. As a result, a device reset is triggered as the watchdog counter overflows the bounded value.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file.

Path of the application within the repository is apps/wdt/wdt_timeout.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32cm_pl10_curiosity_nano.XMPLAB X project for PIC32CM PL10 Curiosity Nano Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameBoard
pic32cm_pl10_curiosity_nano.XPIC32CM PL10 Curiosity Nano Evaluation Kit

Setting Up PIC32CM PL10 Curiosity Nano Evaluation Kit

  • Connect the Debug USB port on the board to the computer using a USB Type-C cable

Running the Application

  1. Open the terminal application (e.g., Tera term) on the computer.
  2. Connect to the Curiosity Virtual COM port and configure the serial settings as follows:
    • Baud: 115200
    • Data: 8 bits
    • Parity: None
    • Stop: 1 bit
    • Flow Control: None
  3. Build and program the application project using its IDE.
  4. LED should be blinking and the console displays the following message:
    Figure 1-7. Terminal Display
  5. Press the switch to put the system in a deadlock.
  6. LED should stop blinking and the console should print the following message:
    Figure 1-8. Terminal Display
  7. WDT will reset the device in four seconds and the demonstration should restart.
  8. Once the demo is completed, do a power on reset to ensure WDT can be disabled for next program.

Refer to the following table for details of Switch and LED:

BoardSwitch NameLED Name
PIC32CM PL10 Curiosity Nano Evaluation KitSW0LED0