1.13 PM Wakeup Using RTC

This example demonstrates entering the Low Power modes and exiting it using the RTC.

Description

The PM peripheral library is used to enter into the Low Power modes, and uses the RTC timer to wake up the device from the Low Power mode. The RTC peripheral is run continuously, including in the device’s low-power sleep modes. The RTC counter value is continuously compared with the Compare registers and generates compare match interrupt when compare match occurs to wake up the device.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file.

Path of the application within the repository is apps/pm/pm_wakeup_rtc.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32cm_pl10_curiosity_nano.XMPLAB X project for PIC32CM PL10 Curiosity Nano Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameBoard
pic32cm_pl10_curiosity_nano.XPIC32CM PL10 Curiosity Nano Evaluation Kit

Setting Up PIC32CM PL10 Curiosity Nano Evaluation Kit

  • Connect the Debug USB port on the board to the computer using a USB Type-C cable

Running the Application

  1. Open the terminal application (e.g., Tera term) on the computer.
  2. Connect to the Curiosity Virtual COM port and configure the serial settings as follows:
    • Baud: 115200
    • Data: 8 bits
    • Parity: None
    • Stop: 1 bit
    • Flow Control: None
  3. Build and program the application using its IDE.
  4. LED is blinked continuously using the SysTick.
  5. The console displays the following message:
  6. Select a or b to enter the Low Power mode (the LED is turned OFF when the device enters Low Power mode).
  7. When the device wakes up on RTC compare match interrupt, the LED starts blinking and the console displays the following message:

Refer to the following table for details of LED:

BoardLED Name
PIC32CM PL10 Curiosity Nano Evaluation KitLED0