1.25 TC Timer Mode
This example shows how to use the TC module in Timer mode to generate periodic interrupt.
Description
TC channel is configured in Timer mode and generates periodic interrupt. LED is toggled in the interrupt handler to indicate periodic callback.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file.
Path of the application within the repository is apps/tc/tc_timer_mode.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32cm_pl10_curiosity_nano.X | MPLAB X project for PIC32CM PL10 Curiosity Nano Evaluation Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| pic32cm_pl10_curiosity_nano.X | PIC32CM PL10 Curiosity Nano Evaluation Kit |
Setting Up PIC32CM PL10 Curiosity Nano Evaluation Kit
- Connect the Debug USB port on the board to the computer using a USB Type-C cable
Running the Application
- Build and program the application using its IDE.
- Observe that the LED blinks once every second.
Refer to the following table for details of LED:
| Board | LED Name |
|---|---|
| PIC32CM PL10 Curiosity Nano Evaluation Kit | LED0 |