Using MPLAB X IDE, follow these steps to download the project files
into the microSDHC card in the MPLAB PICkit
4 and enter Programmer-To-Go mode.
- 1.Insert a formatted
FAT32-compatible microSDHC card into the PICkit 4.
- 2.Ensure that you have the
appropriate connections to the device for Programmer-To-Go:
- PICkit 4
is connected to the computer via the USB cable.
- PICkit 4
is connected via the appropriate programming
interface connector to the target board.
- The
target board is powered from either the PICkit 4 or
a power supply, depending on your Project Properties
selection.
- 3.In MPLAB X IDE, open the
project you want to use and select the PICkit 4 tool for
programming.
- 4.Right-click on your
project name to open the Project Properties dialog. Then click on
PICkit 4 under Categories to display the
Options for PICkit 4 on the right side of the
display. Select the Programmer-To-Go option category.
Figure 1. MPLAB
X IDE Programmer-To-Go Options
- 5.In the Image Name
field, the default is “<your project name>_ptg,” though you
can edit the name, if you wish. This will be the folder name on the
microSDHC card that contains the appropriate files for
Programmer-To-Go.
- 6.In the Send image to
tool, the check box is selected by default. With the box
checked, the PTG image is created and then sent to the microSDHC
card in the connected MPLAB PICkit
4.
- 7.The Program Device
check box is selected by default. When the check box selected, the
device connected to the MPLAB PICkit
4 is programmed.
- 8.Click Apply, then
OK. Use the Make and Program Device Main Project icon
on the toolbar and select Programmer-To-Go PICkit3/PICkit4 Main
Project.
Figure 2. MPLAB
X IDE - Download Image to the MicroSDHC Card
During this process, the device is programmed,
then the microSDHC card is populated with the appropriate
files for the Programmer-To-Go operation. The Output window
displays a status message “Programming/Verify complete” when
the process finishes successfully.
Note: The
PTG settings on the microSDHC card are the same as
in the project (for example, memory, power,
etc.).
The PICkit 4 is
now in Programmer-To-Go mode. The LED should
blink green to indicate the tool has been configured
successfully for Programmer-To-Go.
- 9.Disconnect the PICkit 4
and you’re ready to use Programmer-To-Go.