User Word Programming Sequence
A word programming sequence typically includes the following steps, subject to the constraints externally imposed by the security module:
- Write data to be programmed to NVMDATAx.
 - Load NVMADR with the Flash address to be programmed.
 - Configure NVMCON to word
                        program:
- WREN =
                            
1 - PROGOP = Word program (see NVMCON)
 
 - WREN =
                            
 - Set the WR bit.
 - The program sequence completes and the WR bit is cleared by hardware.
 - Clear WREN bit.
 - Test the WRERR bit to ensure the program sequence completed successfully.
 
Note: Writes to NVMDATAx registers are inhibited while WR = 
        1.