14.4.2.2.4 Center-Aligned PWM Mode
Center-Aligned PWM mode signals avoid coincident rising or falling edges between PWM Generators when the duty cycles are different, reducing excessive current ripple and filtering requirements in power inverter applications.
The PWM pulse maintains symmetry around the end of the first timer
cycle and the beginning of the second cycle. If the duty cycle of the PWM signal is
increased, then the position of the rising edge and the falling edge will change to
maintain this symmetry. Center-Aligned PWM mode is selected when MODSEL[2:0]
(PGxCON[2:0]) = 100. Center-Aligned PWM
operating mode uses two timer cycles to produce a single pulse. The characteristics of the
PWM signal are defined by two SFRs:
- PGxDC: Determines the width of the PWM pulse from the center of the two timer cycles
- PGxPER: Determines the end of the PWM timer count cycle
The falling edge occurs when the PWM Generator Timer = PGxDC, and
the rising edge occurs when the PG Timer = PGxPER – PGxDC + 1. An offset of 1 is added to
the rising edge calculation to produce symmetry between the two timer count cycles. A PGxDC
value of ‘1’, for example, will produce a pulse
that is two cycles in duration. When PGxDC =0, there are restrictions on the maximum PER
value. In standard resolution, the max value is 0xFFFE. If the PER value is above this
value, a short pulse at EOC may occur.
The timer cycle is tracked using the CAHALF status bit (PGxSTAT[1]),
and is read as ‘0’ on the first half of cycle and
‘1’ on the second half. Buffer updates to the
duty cycle or period are allowed only at the beginning of the first timer cycle. The
End-of-Cycle (EOC) interrupt is generated only after the completion of both period cycles.
Figure 14-9 shows the relationship between the
control SFRs and the output waveform. See Data Buffering for additional
information on data buffering.
Center-Aligned mode data restrictions and behavior:
- PHASE must be > 0; if not rising edge will not occur
- PHASE must be < PER; if not falling edge will not occur
- DC must be > 0; if not falling edge will not occur
- DC must be < PER; if not falling edge will not occur, 0% DC
- IF PER=DC, DC is 100%