22.3.2.4 Transmitting Sensor Data
To summarize the following sections, use the following steps and the Sensor Communication Code Example.
- Configure BiSS PPS.
- Configure SCD frequency and getsense frequency.
- Select the client location, the protocol used on the channel and determine if the client device is a sensor or an actuator.
- Configure the SCD length.
- Configure the CRC used and the CRC length.
- Turn the module on.
- Initialize the BiSS module and poll INSTRWA (can read B1SCDATAxX now if line delay calculations are desired later).
- Turn AGS on.
- Poll end of transmission, EOT, Status bit and/or CRC Valid bit to confirm a successful transmission.
- Read value from B1SCDATAxX.