14.5.2 Three-Phase Sinusoidal Control of PMSM/ACIM Motors
Three-phase sinusoidal control applies voltages to the three-phase motor windings, which are Pulse-Width Modulated to produce sinusoidal currents as the motor spins. This eliminates the torque ripple and commutation spikes associated with trapezoidal commutation. Typically, Center-Aligned Complementary PWMs are used for sinusoidal control of a Permanent Magnet Synchronous Motor (PMSM) or three-phase AC Induction Motor (ACIM). Center-aligned PWM signals reduce the level of harmonics in output voltages and currents as compared to edge-aligned PWMs. Three PWM Generators are connected to the three-phase power bridge driving the motor, as shown in Figure 14-39.
PWM Generator 1 is configured as host, and PWM Generator 2 and PWM Generator 3 are configured as client PWMs. PWM configuration used in three-phase sinusoidal control is summarized below:
- PG1-PG3: Uses master period and independent duty cycles
- PG1-PG3: PWM Operating mode is selected as Center-Aligned mode
- PG1-PG3: Configured to operate in Single Trigger mode
- PG1-PG3: PWM Output mode is configured as Complementary Output mode
- PG2-PG3: Uses PG1 trigger output as Start-of-Cycle, whereas PG1 is self-triggered
- PG2-PG3: Enabled during initialization
- PG1 is enabled only after configuring all the control registers; whenever PG1 is enabled, all the generators will start in unison
Figure 14-43 shows the PWM waveforms for a given point in time.
Center-Aligned mode uses two timer cycles to produce a PWM cycle and maintains symmetry
at the center of each PWM cycle. Each timer cycle can be tracked using the status bit,
CAHALF (PGxSTAT[1]), of the respective PWM Generator. The leading edge is produced when
CAHALF = 0 and the falling edge is produced when CAHALF =
1. Note that with Center-Aligned mode, as long as the duty cycles
are different for each phase, the switching instants occur at different times. (In
Edge-Aligned mode, the turn-on times are coincident.) This generally reduces
electromagnetic interference.
Three-Phase Sinusoidal PMSM/ACIM Motor Control Code
void PWMInitialization(void);
int main() {
PWMInitialization();
while(1) {
//Anything to do here?
}
return 0;
}
void PWMInitialization(void) {
//Set PWM master clock to 400MHz from PLL2 through CLKGEN5
configure_PLL2_Fout_400MHz();
clock_PWM_from_PLL2_Fout();
//Set PWM Master Phase Register - No phase shift
MPHASE = 0;
//Set PWM Period (frequency 100kHz, given a 400MHz PWM master clock)
//Note that center-aligned mode takes 2 timer cycles to produce 1 PWM cycle.
MPER = (2000 << 4); //Time units are 1/16 of PWM period
//Set PWM Duty Cycles
PG1DC = (500 << 4); //25%
PG2DC = (1000 << 4); //50%
PG3DC = (1500 << 4); //75%
//Ensure PWM Generators 1-3 are disabled before initializing
PG1CONbits.ON = 0;
PG2CONbits.ON = 0;
PG3CONbits.ON = 0;
//Set Dead Time Registers
PG1DTbits.DTL = (200 << 4); //200 PWM clocks of dead time on PWM1L
PG1DTbits.DTH = (200 << 4); //200 PWM clocks of dead time on PWM1H
PG2DTbits.DTL = (200 << 4); //200 PWM clocks of dead time on PWM2L
PG2DTbits.DTH = (200 << 4); //200 PWM clocks of dead time on PWM2H
PG3DTbits.DTL = (200 << 4); //200 PWM clocks of dead time on PWM3L
PG3DTbits.DTH = (200 << 4); //200 PWM clocks of dead time on PWM3H
PG1CONbits.MDCSEL = 0; //Select PG1DC as PWM Generator 1's duty cycle register
PG1CONbits.MPERSEL = 1; //Select MPER as PWM Generator 1's period register
PG1CONbits.MPHSEL = 1; //Select MPHASE as PWM Generator 1's phase register
PG1CONbits.MSTEN = 1; //PWM Generator 1 broadcasts software set of UPDREQ control bit and EOC signal to other PWM generators.
PG1CONbits.UPDMOD = 0b000; //PWM Buffer Update Mode is at start of next PWM cycle if UPDREQ = 1
PG1CONbits.TRGMOD = 0b00; //PWM generator 1 operates in Single Trigger Mode
PG1CONbits.CLKSEL = 1; //PWM Generator 1 uses PWM Master Clock, undivided and unscaled
PG1CONbits.MODSEL = 0b100; //PWM Generator 1 operates in Center-Aligned mode
PG1CONbits.SOCS = 0b0000; //Start of Cycle is Local EOC
PG1IOCONbits.PMOD = 0b00; //PWM Generator 1 Output operates in Complementary Mode
PG1IOCONbits.PENH = 1; //PWM Generator 1 controls the PWM1H output pin
PG1IOCONbits.PENL = 1; //PWM Generator 1 controls the PWM1L output pin
PG1EVTbits.ADTR1EN1 = 1; //PGxTRIGA register compare event is enabled as trigger source for ADC Trigger 1
PG1EVTbits.UPDTRG = 0b01; //A write of the PGxDC register automatically sets the UPDREQ bit
PG1EVTbits.PGTRGSEL = 0b000; //PWM generator trigger output is EOC
PG2CONbits.MDCSEL = 0; //Select PG2DC as PWM Generator 2's duty cycle register
PG2CONbits.MPERSEL = 1; //Select MPER as PWM Generator 2's period register
PG2CONbits.MPHSEL = 1; //Select MPHASE as PWM Generator 2's phase register
PG2CONbits.MSTEN = 0; //PWM generator 2 does not broadcast UPDATE status bit or EOC signal to other PWM generators
PG2CONbits.UPDMOD = 0b011; //PWM Buffer Update Mode is client immediate
PG2CONbits.TRGMOD = 0b00; //PWM generator 2 operates in Single Trigger Mode
PG2CONbits.SOCS = 0b0001; //Start of Cycle is PG1 trigger output selected by PG1EVTbits.PGTRGSEL<2:0> bits
PG2CONbits.CLKSEL = 1; //PWM Generator 2 uses PWM Master Clock, undivided and unscaled
PG2CONbits.MODSEL = 0b100; //PWM Generator 2 operates in Center-Aligned mode
PG2IOCONbits.PMOD = 0b00; //PWM Generator 2 output operates in Complementary Mode
PG2IOCONbits.PENH = 1; //PWM Generator 2 controls the PWM2H output pin
PG2IOCONbits.PENL = 1; //PWM Generator 2 controls the PWM2L output pin
PG3CONbits.MDCSEL = 0; //Select PG3DC as PWM Generator 3's duty cycle register
PG3CONbits.MPERSEL = 1; //Select MPER as PWM Generator 3's period register
PG3CONbits.MPHSEL = 1; //Select MPHASE as PWM Generator 3's phase register
PG3CONbits.MSTEN = 0; //PWM generator 3 does not broadcast UPDATE status bit or EOC signal to other PWM generators
PG3CONbits.UPDMOD = 0b011; //PWM Buffer Update Mode is client immediate
PG3CONbits.TRGMOD = 0b00; //PWM generator 3 operates in Single Trigger Mode
PG3CONbits.SOCS = 0b0001; //Start of Cycle is PG1 trigger output selected by PG1EVTbits.PGTRGSEL<2:0> bits
PG3CONbits.CLKSEL = 1; //PWM Generator 3 uses PWM Master Clock, undivided and unscaled
PG3CONbits.MODSEL = 0b100; //PWM Generator operates in Center-Aligned mode
PG3IOCONbits.PMOD = 0b00; //PWM Generator 3 output operates in Complementary Mode
PG3IOCONbits.PENH = 1; //PWM Generator 3 controls the PWM3H output pin
PG3IOCONbits.PENL = 1; //PWM Generator 3 controls the PWM3L output pin
//Enable all PWM generators; PWM generator 1 will start the sequence