4.9.6.3 Alternate Port Functions
In addition to being general digital I/Os, most port pins have alternate functions. The following figure illustrates how the port pin control signals from the simplified General Digital I/O can be overridden by alternate functions. See General Digital I/O in the Ports as General Digital I/O from Related Links. The overriding signals may not be present in all port pins, but the figure serves as a generic description applicable to all port pins in the AVR microcontroller.
WRx, WPx, WDx, RRx, RPx and RDx are common to all pins within the same port. CLKI/O, SLEEP and PUD are common to all ports. All other signals are unique for each pin.
The following table summarizes the function of the overriding signals. The pin and port indices are not shown in the tables below. The overriding signals are generated internally in the modules that have the alternate function.
Signal Name | Full Name | Description |
|---|---|---|
PUOE | Pull-Up Override Enable | If this signal is set, the pull-up enable is controlled by the PUOV signal. If this signal is cleared, the pull-up is enabled when {DDxn, PORTxn, PUD} = 0b010. |
PUOV | Pull-Up Override Value | If PUOE is set, the pull-up is enabled/disabled when PUOV is set/cleared, regardless of the setting of the DDxn, PORTxn and PUD register bits. |
DDOE | Data Direction Override Enable | If this signal is set, the output driver enable is controlled by the DDOV signal. If this signal is cleared, the output driver is enabled by the DDxn register bit. |
DDOV | Data Direction Override Value | If DDOE is set, the output driver is enabled/disabled when DDOV is set/cleared, regardless of the setting of the DDxn register bit. |
PVOE | Port Value Override Enable | If this signal is set and the output driver is enabled, the port value is controlled by the PVOV signal. If PVOE is cleared, and the output driver is enabled, the port value is controlled by the PORTxn register bit. |
PVOV | Port Value Override Value | If PVOE is set, the port value is set to PVOV, regardless of the setting of the PORTxn register bit. |
PTOE | Port Toggle Override Enable | If PTOE is set, the PORTxn register bit is inverted. |
DIEOE | Digital Input Enable Override Enable | If this bit is set, the digital input enable is controlled by the DIEOV signal. If this signal is cleared, the digital input enable is determined by MCU state (normal mode, sleep mode). |
DIEOV | Digital Input Enable Override Value | If DIEOE is set, the digital input is enabled/disabled when DIEOV is set/cleared, regardless of the MCU state (normal mode, sleep mode). |
DI | Digital Input | This is the digital input to alternate functions. In the preceding figure, the signal is connected to the output of the Schmitt trigger but before the synchronizer. Unless the digital input is used as a clock source, the module with the alternate function uses its own synchronizer. |
AIO | Analog Input/Output | This is the analog Input/Output to/from alternate functions. The signal is connected directly to the pad and can be used bi-directionally. |
The following subsections briefly describe the alternate functions for each port and explain the relation of the overriding signals to the alternate function.
Alternate Functions of PORTB
PORTB pins with alternate functions are shown in the following table and described in more detail farther below.
Port Pin | Alternate Functions |
|---|---|
PB7 | NPWRON6 (not power-on number 6) PCINT7 (pin change interrupt 7) RX_ACTIVE (strong high-side driver) LED0 (strong low-side driver) Switchable pull-up resistor |
PB6 | PCINT6 (pin change interrupt 6) EVENT (firmware controlled event to external microcontroller) Switchable pull-up resistor |
PB5 | PCINT5 (pin change interrupt 5) INT1 (external Interrupt 1) NSS (SPI bus host client select) Switchable pull-up resistor |
PB4 | PWRON (power-on) PCINT4 (pin change interrupt 4) LED1 (strong high-side driver) Switchable pull-up resistor |
PB3 | PCINT3 (pin change interrupt 3) MISO (SPI bus host input/client output) Switchable pull-up resistor |
PB2 | PCINT2 (pin change interrupt 2) MOSI (SPI bus host output/client input) Switchable pull-up resistor |
PB1 | PCINT1 (pin change interrupt 1) SCK (SPI bus host output clock/client input clock) Switchable pull-up resistor |
PB0 | PCINT0 (pin change interrupt 0) CLK_OUT (reference clock output) Switchable pull-up resistor |
PB7 – PORTB, Bit 7
NPWRON6 – Low active power-on signal. Enables the DVCC power supply.
PCINT7 – Pin change interrupt source 7: The PB7 pin can serve as an external interrupt source.
RX_ACTIVE – Firmware controlled, hardware supported function: This indicates that the receiver is active. The pin has a strong low-side driver that can provide more current than the usual pins to supply an external LNA. The high-side driver is enabled on demand by the MCUCR.PB7HS bit. See I/O Ports Register Description from Related Links. It can also be used to drive an external LED. For figures about drive strength, refer to the ATA8210/ATA8215 UHF ASK/FSK Receiver Data Sheet (9344E).
LED0 – The pin has a strong low-side driver that can provide more current than the usual pins to supply an external LED. The low-side driver is enabled on demand by the MCUCR.PB7LS bit. See I/O Ports Register Description from Related Links. For figures about drive strength, refer to the ATA8210/ATA8215 UHF ASK/FSK Receiver Data Sheet (9344E).
PB6 – PORTB, Bit 6
PCINT6 – Pin change interrupt source 6: The PB6 pin can serve as an external interrupt source.
EVENT – Firmware function: Event signalization to external microcontroller. It indicates an important change in the receiver state; for example, valid data detected.
PB5 – PORTB, Bit 5
PCINT5 – Pin change interrupt source 5: The PB5 pin can serve as an external interrupt source.
INT1 – External interrupt 1.
NSS – Not client port select input. When the SPI is enabled as a client, this pin is configured as an input regardless of the DDB5 setting. As a client, the SPI is activated when this pin is driven low. When the SPI is enabled as a host, the data direction of this pin is controlled by DDB5. When the pin is forced to be an input, the pull-up resistor can still be controlled by the PORTB5 bit.
PB4 – PORTB, Bit 4
PWRON – High active power-on signal. Enables the DVCC power supply.
PCINT4 – Pin change interrupt source 4: The PB4 pin can serve as an external interrupt source.
LED1 – The pin has a strong high-side driver that can provide more current than the usual pins to supply an external LED. The high-side driver is enabled on demand by the MCUCR.PB4HS bit. See I/O Ports Register Description from Related Links. For figures about drive strength, refer to the ATA8210/ATA8215 UHF ASK/FSK Receiver Data Sheet (9344E).
PB3 – PORTB, Bit 3
PCINT3 – Pin change interrupt source 3: The PB3 pin can serve as an external interrupt source.
MISO – SPI host data input, client data output for SPI channel. When the SPI is enabled as a host, this pin is configured as an input regardless of the DDB3 setting. When the SPI is enabled as a client, the data direction of this pin is controlled by DDB3. When the pin is forced to be an input, the pull-up resistor can still be controlled by the PORTB3 bit.
PB2 – PORTB, Bit 2
PCINT2 – Pin change interrupt source 2: The PB2 pin can serve as an external interrupt source.
MOSI – Host data output, client data input pin for SPI channel. When the SPI is enabled as a client, this pin is configured as an input regardless of the DDB2 setting. When the SPI is enabled as a host, the data direction of this pin is controlled by DDB2. When the pin is forced to be an input, the pull-up resistor can still be controlled by the PORTB2 bit.
PB1 – PORTB, Bit 1
PCINT1 – Pin change interrupt source 1: The PB1 pin can serve as an external interrupt source.
SCK – Host clock output, client clock input pin for SPI channel. When the SPI is enabled as a client, this pin is configured as an input regardless of the DDB1 setting. When the SPI is enabled as a host, the data direction of this pin is controlled by DDB1. When the pin is forced to be an input, the pull-up resistor can still be controlled by the PORTB1 bit.
PB0 – PORTB, Bit 0
PCINT0 – Pin change interrupt source 0: The PB0 pin can serve as an external interrupt source.
CLK_OUT – A divided XTO, ADC or RC oscillator clock can be output on this pin as a reference clock for an external microcontroller. See System Clock and Clock Options from Related Links. The corresponding data direction register of the port has to be set as output to enable the driver.
OFFMode Behavior of PORTB
The PORTB functions for the OFFMode are hardwired.
All port pins of PORTB are inputs in the OFFMode. PB0 to PB6 have no internal pull-up resistor.
Port Pin | Internal Pull- Up | OFFMode Function |
|---|---|---|
PB7 | Yes | NPWRON6 (low active) |
PB6 | No | Floating input. Port circuitry avoids internal transverse current. |
PB5 | No | Floating input. Port circuitry avoids internal transverse current. |
PB4 | No | PWRON (high active) Input level must be defined by external circuitry to avoid unwanted wake-ups and transverse current. Ground level (low) is required to be able to use the OFFMode. |
PB3 | No | Floating input. Port circuitry avoids internal transverse current. |
PB2 | No | MOSI Input level must be defined by external circuitry to avoid internal transverse current in the port. |
PB1 | No | SCK Input level must be defined by external circuitry to avoid internal transverse current in the port. |
PB0 | No | Floating input. Port circuitry avoids internal transverse current. |
Alternate Functions of PORTC
Port C pins with alternate functions are shown in the following table and described in more detail farther below.
Port Pin | Alternate Functions |
|---|---|
PC5 | NPWRON5 (not power-on number 5) PCINT13 (pin change interrupt 13) TMDO_CLK (transparent mode data clock output) TRPB (transparent RX path B data) Switchable pull-up resistor |
PC4 | NPWRON4 (not power-on number 4) PCINT12 (pin change interrupt 12) RxD (Timer 3 input for 1 wire bus decoding) INT0 (external interrupt 0) Switchable pull-up resistor |
PC3 | NPWRON3 (not power-on number 3) PCINT11 (pin change interrupt 11) TMDO (transparent data output) TxD (TM1 output for 1 wire bus) Switchable pull-up resistor |
PC2 | NPWRON2 (not power-on number 2) PCINT10 (pin change interrupt 10) TRPA (transparent RX path A data) Switchable pull-up resistor |
PC1 | NPWRON1 (not power-on number 1) PCINT9 (pin change interrupt 9) Switchable pull-up resistor |
PC0 | PCINT8 (pin change interrupt 8) NRESET (low active microcontroller reset) debugWIRE (on-chip debug interface) Switchable pull-up resistor |
PC5 – PORTC, Bit 5
NPWRON5 – Low active power-on signal. Enables the DVCC power supply.
PCINT13 – Pin change interrupt source 13: The pin can serve as an external interrupt source.
TMDO_CLK – Transparent mode data clock output. Provides a sampling clock for the transparent mode data output (TMDO pin). It can be used to clock the data with the rising clock edge into a receiving shift register. TMDO_CLK has priority over the TRPB output function.
TRPB – The raw data of the transparent receiving path B is provided to an external microcontroller for decoding. The corresponding data direction register of the port has to be set as output to enable the driver. TRPB has lower priority than TMDO_CLK.
PC4 – PORTC, Bit 4
NPWRON4 – Low active power-on signal. Enables the DVCC power supply.
PCINT12 – Pin change interrupt source 12: The pin can serve as an external interrupt source.
RXD – Use as an input for Timer3. This allows data decoding from the 1 wire bus interface. This feature is not included in the firmware library.
INT0 – External interrupt 0.
PC3 – PORTC, Bit 3
NPWRON3 – Low active power-on signal. Enables the DVCC power supply.
PCINT11 – Pin change interrupt source 11: The pin can serve as an external interrupt source.
TMDO – Transparent mode data output (RX). Decoded and spike-free ASK or FSK data can be multiplexed to this port. The corresponding data direction register of the port has to be set as output to enable the driver. TMDO has priority over the TxD output function.
TxD – TX modulator data output: The TX modulator I/O interface can be used to provide the modulation for the 1 wire bus interface. The PC3 pin can serve as an external out for the TX modulator. The function of the modulator output pin is dependent on the TX modulator port interface select bits (TMPIS[2:0]) in the TMCR1 register. The PC3 pin has to be configured as an output (DDC3 set to ‘1’) to serve this function. TxD has lower priority than TMDO.
PC2 – PORTC, Bit 2
NPWRON2 – Low active power-on signal. Enables the DVCC power supply.
PCINT10 – Pin Change Interrupt Source10: The pin can serve as an external interrupt source.
TRPA – The raw data of the transparent receiving path A is provided to an external microcontroller for decoding. The corresponding data direction register of the port has to be set as output to enable the driver.
PC1 – PORTC, Bit 1
NPWRON1 – Low active power-on signal. Enables the DVCC power supply.
PCINT9 – Pin change interrupt source 9: The pin can serve as an external interrupt source.
PC0 – PORTC, Bit 0
PCINT8 – Pin change interrupt source 8: The pin can serve as an external interrupt source.
NRESET – Can be configured by fuse settings as an nreset input for the AVR. If the nreset functionality is enabled, a low level on this pin for longer than 10 µs generates a reset, even if the clock is not running. Shorter pulses could also trigger a reset.
debugWIRE – debugWIRE interface for in-circuit debugging.
OFFMode Behavior of PORTC
The port C functions for the OFFMode are hardwired. All port pins of PORTC are inputs in OFFMode.
Port Pin | Internal Pull-up | OFFMode Function |
|---|---|---|
PC5 | YES | NPWRON5 (low active) |
PC4 | YES | NPWRON4 (low active) |
PC3 | YES | NPWRON3 (low active) |
PC2 | YES | NPWRON2 (low active) |
PC1 | YES | NPWRON1 (low active) |
PC0 | YES | NRESET if activated by fuse |