4.9.3.4 I/O Memory
For more details about the I/O memory space definition, see Register Map from Related Links.
All AVR I/O modules and peripherals are placed in the I/O space. All I/O locations may be accessed by the LD/LDS/LDD and ST/STS/STD instructions, transferring data between the 32 general purpose working registers and the I/O space. I/O registers within the address range 0x00 – 0x1F are directly bit-accessible using the SBI and CBI instructions. In these registers, the value of single bits can be checked by using the SBIS and SBIC instructions. Refer to the instruction set section for more details.
When using the I/O specific commands IN and OUT, the I/O addresses 0x00 – 0x3F must be used. When addressing I/O registers as data space using LD and ST instructions, 0x20 must be added to these addresses. The AVR is a complex microcontroller with more peripheral units than can be supported within the 64 location reserved in op-code for the IN and OUT instructions. For the extended I/O space from 0x60 – 0x1FF and the SRAM, only the ST/STS/STD and LD/LDS/LDD instructions can be used.
For compatibility with future devices, reserved bits must be written to ‘0’
if accessed. Reserved I/O memory addresses must never be written.
Some of the status flags are cleared by writing a logical ‘1’ to them. Note
that the CBI and SBI instructions only operate on the specified bit and can therefore be used
on registers containing such status flags. The CBI and SBI instructions work with registers
0x00 to 0x1F only.
The I/O and peripherals control registers are explained in later sections.