6.20.21 strspn Function
Calculate the number of consecutive characters at the beginning of a string that are contained in a set of characters.
Include
<string.h>
Prototype
size_t strspn(const char *s1, const char
*s2);
Arguments
s1- pointer to the string to be searched
s2- pointer to characters to search for
Return Value
Returns the number of consecutive characters from the beginning of
s1 that are contained in s2.
Remarks
This function stops searching when a character from s1 is
not in s2.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <string.h>
#include <stdio.h>
int main(void)
{
char str1[20] = "animal";
char str2[20] = "aeiounm";
char str3[20] = "aimnl";
char str4[20] = "xyz";
int res;
res = strspn(str1, str2);
printf("strspn(\"%s\", \"%s\") = %d\n",
str1, str2, res);
res = strspn(str1, str3);
printf("strspn(\"%s\", \"%s\") = %d\n",
str1, str3, res);
res = strspn(str1, str4);
printf("strspn(\"%s\", \"%s\") = %d\n",
str1, str4, res);
}
Example Output
strspn("animal", "aeiounm") = 5
strspn("animal", "aimnl") = 6
strspn("animal", "xyz") = 0
Example Explanation
In the first result, l is not in s2.
In the second result, the terminating null is not in s2.
In the third result, a is not in s2 , so
the comparison stops.