6.20.22 strstr Function
Search for the first occurrence of a string inside another string.
Include
<string.h>
Prototype
char *strstr(const char *s1, const char
*s2);
Arguments
s1- pointer to the string to be searched
s2- pointer to substring to be searched for
Return Value
Returns the address of the first element that matches the substring if found; otherwise, returns a null pointer.
Remarks
This function will find the first occurrence of the string
s2 (excluding the null terminator) within the string
s1. If s2 points to a zero length string,
s1 is returned.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <string.h>
#include <stdio.h>
int main(void)
{
char str1[20] = "What time is it?";
char str2[20] = "is";
char str3[20] = "xyz";
char *ptr;
int res;
printf("str1 : %s\n", str1);
printf("str2 : %s\n", str2);
printf("str3 : %s\n\n", str3);
ptr = strstr(str1, str2);
if (ptr != NULL)
{
res = ptr - str1 + 1;
printf("\"%s\" found at position %d\n",
str2, res);
}
else
printf("\"%s\" not found\n", str2);
printf("\n");
ptr = strstr(str1, str3);
if (ptr != NULL)
{
res = ptr - str1 + 1;
printf("\"%s\" found at position %d\n",
str3, res);
}
else
printf("\"%s\" not found\n", str3);
}
Example Output
str1 : What time is it?
str2 : is
str3 : xyz
"is" found at position 11
"xyz" not found