6.20.19 strpbrk Function
Search a string for the first occurrence of a character from a specified set of characters.
Include
<string.h>
Prototype
char *strpbrk(const char *s1, const char
*s2);
Arguments
s1- pointer to the string to be searched
s2- pointer to characters to search for
Return Value
Returns a pointer to the matched character in s1 if found;
otherwise, returns a null pointer.
Remarks
This function will search s1 for the first occurrence of a
character contained in s2.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <string.h>
#include <stdio.h>
int main(void)
{
char str1[20] = "What time is it?";
char str2[20] = "xyz";
char str3[20] = "eou?";
char *ptr;
int res;
printf("strpbrk(\"%s\", \"%s\")\n", str1, str2);
ptr = strpbrk(str1, str2);
if (ptr != NULL)
{
res = ptr - str1 + 1;
printf("match found at position %d\n", res);
}
else
printf("match not found\n");
printf("\n");
printf("strpbrk(\"%s\", \"%s\")\n", str1, str3);
ptr = strpbrk(str1, str3);
if (ptr != NULL)
{
res = ptr - str1 + 1;
printf("match found at position %d\n", res);
}
else
printf("match not found\n");
}
Example Output
strpbrk("What time is it?", "xyz")
match not found
strpbrk("What time is it?", "eou?")
match found at position 9