6.20.9 strchr Function
Locates the first occurrence of a specified character in a string.
Include
<string.h>
Prototype
char *strchr(const char *s, int c);
Arguments
s- pointer to the string
c- character to search for
Return Value
Returns a pointer to the location of the match if successful; otherwise, returns a null pointer.
Remarks
This function searches the string s to find the first
occurrence of the character, c.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <string.h>
#include <stdio.h>
int main(void)
{
char buf1[50] = "What time is it?";
char ch1 = 'm', ch2 = 'y';
char *ptr;
int res;
printf("buf1 : %s\n\n", buf1);
ptr = strchr(buf1, ch1);
if (ptr != NULL)
{
res = ptr - buf1 + 1;
printf("%c found at position %d\n", ch1, res);
}
else
printf("%c not found\n", ch1);
printf("\n");
ptr = strchr(buf1, ch2);
if (ptr != NULL)
{
res = ptr - buf1 + 1;
printf("%c found at position %d\n", ch2, res);
}
else
printf("%c not found\n", ch2);
}
Example Output
buf1 : What time is it?
m found at position 8
y not found