6.20.23 strtok Function
Break a string into substrings, or tokens, by inserting null characters in place of specified delimiters.
Include
<string.h>
Prototype
char *strtok(char *s1, const char
*s2);
Arguments
s1- pointer to the null terminated string to be searched
s2- pointer to characters to be searched for (used as delimiters)
Return Value
Returns a pointer to the first character of a token (the first character in a sequence of
characters in s1 that does not appear in the set of characters of
s2). If no token is found, the null pointer is returned.
Remarks
A sequence of calls to this function can be used to
split up a string into substrings (or tokens) by replacing specified
characters with null characters. The first time this function is
invoked on a particular string, that string should be passed in
s1. After the first time, this function can
continue parsing the string from the last delimiter by invoking it
with a null value passed in s1.
It skips all leading characters that appear in the string s2
(delimiters), then skips all characters not appearing in s2 (this
segment of characters is the token), and then overwrites the next character with a null
character, terminating the current token. The function, strtok, then
saves a pointer to the character that follows, from which the next search will start. If
strtok finds the end of the string before it finds a delimiter, the
current token extends to the end of the string pointed to by s1. If
that was the first call to strtok, it does not modify the string (no
null characters are written to s1). The set of characters that is
passed in s2 need not be the same for each call to
strtok.
If strtok is called with a non-null
parameter for s1 after the initial call, the string
becomes the new string to search. The old string previously searched
will be lost.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <string.h>
#include <stdio.h>
int main(void)
{
char str1[30] = "Here, on top of the world!";
char delim[5] = ", .";
char *word;
int x;
printf("str1 : %s\n", str1);
x = 1;
word = strtok(str1,delim);
while (word != NULL)
{
printf("word %d: %s\n", x++, word);
word = strtok(NULL, delim);
}
}
Example Output
str1 : Here, on top of the world!
word 1: Here
word 2: on
word 3: top
word 4: of
word 5: the
word 6: world!